This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25700不充电问题



你好,我现在在使用BQ25700A芯片,输入是TYPE-C的5V,输出是4.2V的锂电池,接上电池然后接充电器不能充电,然后配置的参数是如下的
0x12 地址写入0x0e22
0x35 地址写入0xffe0
0x15 地址写入0x7010
0x14 地址写入0x0108
0x3d 地址写入0xc013
0x3f 地址写入0x3f 1
配置完成后没有充电电流,读取状态寄存器值如下
0x20: 0xaa
0x21: 0x0
0x22: 0x41
0x23: 0xd1b
0x24: 0x0
0x25: 0xa
0x26: 0xe1b
请问配置是否有问题