This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2733方案测试负载纹波数据

Other Parts Discussed in Thread: LM2733

您好!

我们采用LM2733分别做了5V升12V、12V升15V、12V升18V、12V升35V的应用,并且做了一些负载纹波测试,您看下这些数据对不对?

 

满载(mV)

半载<--->满载(mV)

空载<--->满载(mV)

5V升12V

32

254

1240

12V升15V

37.2

536

2160

12V升18V

39.6

616

2640

12V升35V

61.6

744

3480