bqStudio导入gg.csv后,发现没有校准数据,校准数据还是原始值,gg.csv文件中是存在校准数据的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请参考下面的步骤再一下写入gg文件
When you export the Data Memory, the calibration information is included along with all of the other data flash settings. This can be exported to a .gg.csv file or by using the Hex Dump button.
When you import a .gg.csv file into BQStudio, it will normally not load the calibration data. This is in case you want to run calibration for each device individually. You can change this setting so that calibration can be imported with the following steps:
- Go to Window-> Preferences-> All Global Settings
- Click 'Show Advanced Views' and then click 'Apply'
- On the Data Memory screen, Select 'Import'-> 'Import from File (Advance)'
- Select your file. A window will pop up (Import Dialog). Click 'Configure Selection' in this window
- Here you can check the Calibration box so that calibration settings are also loaded when you import the file.