This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于tps40304的疑惑

Other Parts Discussed in Thread: TPS40304

 准备用TPS40304做降压电源,输入电压是5V,输出电压是3.3V,输出电流最大15A。

有以下几个问题不清楚:

1、5V输入时BP脚(pin 10)的电压是多少?驱动下桥MOS管的时候,LDRV脚(pin 9)输出电压满足要求吗?

2、HDRV脚(pin 7)和LDRV脚(pin 9)与各自驱动的MOS管栅极之间需要串联低阻值的电阻吗?(文档slvr564的原理图中串联了3.3欧电阻,用webanch仿真的时候却没有串联电阻。)

3、补偿回路(pin 4和pin 5)的阻容参数如何计算?(文档slvr564的原理图中参数值与webanch仿真的参数值不一样。)

谢谢!