您好,那请问您目前只有一个220V转9V的适配器,如何设计正负5V,正负18V的电源呢?正负五伏的电流可能要大些,因为要带十几个运放呢。谢谢您的帮助
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,那请问您目前只有一个220V转9V的适配器,如何设计正负5V,正负18V的电源呢?正负五伏的电流可能要大些,因为要带十几个运放呢。谢谢您的帮助
如果贵司的这个项目对成本和PCB面积要求比较严格,由9v得到+-5v的DC_DC转换器可以考虑类似于TPS61080这样单颗芯片同时实现正负电压输出,其方法是选择一个buck转换器,让其buck电路工作于CCM模式下,同时将这个PWm信号接到一个inverting的拓扑,这个inverting需要工作在DCM模式下,inverting在固定的开关频率下,最大负载时的输出电压由其电感决定(可以在这个输出端加一个齐纳二极管进一步的抑制负载变化带来的输出电压波动,这个二极管在设定的最大负载电流时不会导通,所以运行在设定的最大负载时并不影响效率,当负载变小时才会自动分流),输出电压不受输入电压的变化影响(当buck电路由于输入电压增加而减少的占空比与此时工作于DCM模式下的inverting 架构需要减小的占空比相等时,就会自动进行线性调整),只受到inverting本身负载变化的影响,所以对于负载变化比较小的时候这个方案是可行的。这也是一个节约成本和节约PCB面积的选择。
其原理是因为inverting的DCM 输入与输出关系表明,Vo正比于D*D*Vin*Vin(去掉其他常数),而buck电路在CCM模式下D正比于1/Vin,所以用工作于CCM模式下的buck电路的PWM信号驱动工作于DCM模式下的inverting电路,得到的输出电压不再与Vin发生联系(可以看到将Buck模式下的D代入到DCm模式下的Inverting架构后,VO是常数)
总结起来,如果-5V负载电流不是很非常大,可以进入invernting架构的DCM模式,同时负载变化不大,则可以用单颗降压buck芯片工作于CCM模式下的PWM信号来同时驱动外部的一个Inverting架构得到负电压(Vo=D*D*Vin*Vin*10^6/2*Io*L*f,L单位为uH,f单位为HZ)。