This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求几款恒压恒流设计电路



恒压恒流源:要求DC 输入6~8.4V,最大放电电流不低于30A,输出电压5V,电流20A-25A,负载LED列阵,工作时间0.1-0.3S,周期为1S,闪烁,输出恒流25A.

  • Hi
    TI的LED 驱动芯片应该是没有合适,大部分芯片LED设计电流都不是很大,有些外置MOS可以将电流做大,但是输入电压又难以符合。
    建议采用DC/DC芯片来做,主要就是外用额外的电流sense电路(一般可以用运放)来做,相对选择会比较多一些。