This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116使用一段时间后上下MOS管烧毁

Other Parts Discussed in Thread: LM5116

请教大神,我用LM5116做了一个BUCK电流,设计输入电压8~95V,输出电流4A,实际应用输入电压20~32V,输出电流最大2.5A(脉冲峰值电流),实验室应用测试一切正常,带载情况下测试驱动电路波形带有一些振铃,且振铃幅度随负载变大而变大。目前客户现场有1K pcs数量的产品在实际应用中,反馈有2PCS异常,异常状态为5116的上下MOS管烧毁,GSD三个引脚均互相短路,外观无异常,前端保险丝烧断。请教下,什么情况下会导致MOS管烧毁,上下管驱动电路出现振铃会导致MOS管烧毁吗?另外,该电路地给外部器件供电(共地),其中一个器件的地网络接了外框,该外框紧贴系统PE壳体,就相当于5116的地贴了PE外壳,这是否会导致MOS管烧毁?