This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25619RTWR最大充电电流



最大充电电流是多少?如何设置的,下面是充电寄存器的设置:

Fast charge current setting
Default: 340 mA (010001)
Range: 0 mA (0000001) –
1180 mA (111011), 20
mA/step
111100: 1290 mA
111101: 1360 mA
111100: 1430 mA
111100: 1500 mA
ICHG 0 mA disables charge.

为什么111100对应几个充电电流?