This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610充电充不满



电池组是6串1并(单节电池3000mA容量),输入电压28V,设置充电电流是1A,终止充电电流0.3A,现在无法充满 ,充电从18V一直1A充电,但到了24.7V左右时充电电流立即将为0,停止充电,
CE TTC都是高电平VREF,STAT1 指示灯闪烁,HIDRV 电压与电池电压一致24.7V左右