This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542开启QEN,再下命令21无法关闭QEN



BQ27542g1 开启QEN,再下命令21无法关闭QEN

  • 您好,QEN set以后不能清除,请参考下面文档的描述。
    15.1.1.23 IT ENABLE: 0x0021
    Forces the fuel gauge to begin the Impedance Track algorithm, sets Bit 2 of UpdateStatus and causes
    the [VOK] and [QEN] flags to be set in the CONTROL_STATUS register. [VOK] is cleared if the voltages
    are not suitable for a Qmax update. Once set, [QEN] cannot be cleared. This command is only available
    when the fuel gauge is UNSEALED and is typically enabled at the last step of production after system test
    is completed.