This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问给CC3220模块供电,用什么电源芯片?



   电源是20V左右的锂电池,板子比较小,dcdc芯片开关频率是否会干扰wifi信号?

LDO是否效率太低?压差太大。

dcdc和ldo各有什么推荐的,谢谢

  • HI
    输入电压太高,直接用LDO肯定不行,功耗太大,效率太低,可以用DC/DC+LDO来实现。
    射频DC/DC印象中输入电压也不高(TI以前有专门分出这一类芯片,后来取消了,都找不到)
    你可以在CC3220的官网找一下电源推荐方案,但是应该是低压转换方案。 建议是需要增加一个DC/DC先降压。
  • DC/DC的开关频率是否对wifi无线通信有干扰,我主要是担心这个,第一次搞这个,也没有经验。TI的板子里到是用DC/DC的,不过最大输入电压是17V的,关键是这颗电源先给仿真器芯片供电,再给wifi模块供电,距离也比较远,估计有个5,6cm的样子,而我的板子它们的距离要在1cm以内了。
  • HI
    会有干扰得,所以一般必须用射频DC/DC,或者LDO. (有些射频DC/DC也集成了LDO或者负载开关)
    但是你得输入电压很高,需要增加一级DC/DC,不建议直接用LDO(效率太低,功耗大)。
    距离远,可以增加磁珠构成CLC滤波。