Other Parts Discussed in Thread: BQ76940, BQ76930
BQ76930 BQ76940 分别用于10串、13串的两个项目,量产后发现电池包库存一段时间后,BQ76930的第10串,BQ76940的10串12串和13串电池漏电,分析发现AFE的相邻的采样引脚存在漏电,可以确认电池包入库时AFE是没有漏电问题的(如果入库时AFE的采样引脚就存在漏电,1K的采样滤波电阻就会存在压差,上位机可以检测出来),不良的保护板断电后静置1小时,再重新上电,多数情况下之前AFE漏电的故障会消失,但是静置工作一段时间后(可能是10分钟,也可能是1天),故障又会复现,漏电电流呈现逐渐变大的情况,1K的采样滤波电阻上出现电压,采样电压会小于实际电池的电压,AFE输出的电压和AFE采样引脚的电压相同(AFE内部AD采样还是正常的),目前电压采样端口没有加TVS保护二极管,想知道AFE具体的损坏环节,有没有人也遇到过这样的问题,怎么解决的?谢谢!