我使用的电池容量是24Ah,2A电流校准时,只把电流校准为1A,这样充满容量就是12Ah,单片机在读取容量信息时将读到的容量乘以2就是24Ah。
但是现在我遇到一个问题,就是在常温下充放电,读到的电池容量在24Ah以上。高温实验55℃:在高温箱待3个小时以4.8A电流开始放电,整个放电过程大于5小时,放完电在常温下静置超过5个小时,在常温下第一次充电,部分电池容量就有可能充不满,容量可能是18Ah,22Ah,23Ah。然后给电池通过电阻放电放电电流在1.8A--1.3A之间,放完电静置54分钟后开始充电,第二次大部分电池容量均充不满,容量在22Ah-24Ah之间,不大于24Ah。不知道有没有哪位遇到这样的问题,是怎么解决的。