This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53319输出电流问题

Other Parts Discussed in Thread: TPS53319

您好:

       在应用TPS53319时,BUCK下管的RC吸收回路(R=0,C=2.2nF)会影响输出电流,比如:输出3.3A以下正常,但负载加大后,输出关闭,无输出;把RC吸收回路删除,负载加载在8.5A输出依然正常。下图红色框内为RC吸收回路(RW15,RW16,CW40)。

问题:RC吸收回路为什么会影响输出电流的大小?盼答复,谢谢!

  • Hi
    sw脚是不能有较大的寄生参数,这个可能影响到OCP过载保护。 增加RC本身是要消除这里的震荡,而直接加电容显然反而恶化了。一般这里应该是小电阻小电容(不会是0ohm电阻,电容2.2nF应该是偏大的)