This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR16030PDDAR方案,输出电压不正常



LMR16030PDDAR方案,输入43-54V,输出24V/2A,使用官方WEB设计,实际焊接测试发现输出电压只有15V,FB反馈引脚只有0.47V,按照规格书应该是0.75V,使用的是四层板布线。

请问是什么原因造成的?

RT电阻是41.2K,电感是12uH,反馈分压电阻分别是316K和10.2K(官方推荐)。

PGOOD焊盘悬空。