用LM5175 做一个充电器,希望输出电压可以设置,输出电流也可以设置,设置的参考信号是一个可调整的电压源,输入调整范围10-30V,输出电压调整范围:5--25V,电流调整范围1--20A,功率最大500W,输入的电流限制也为20A,选用LM5175 是否可行?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用LM5175 做一个充电器,希望输出电压可以设置,输出电流也可以设置,设置的参考信号是一个可调整的电压源,输入调整范围10-30V,输出电压调整范围:5--25V,电流调整范围1--20A,功率最大500W,输入的电流限制也为20A,选用LM5175 是否可行?
好的,谢谢!
不过 我的输入和输出电流都会被限制到20A,这样应该容易控制一点。
如果按20A设计,我的补偿点应该怎么选择呢。
是否最后的设计的结果补偿回路百特图有45度的余量就可以。