这个IC谁用过,做出来的能否兼容大多电子变压器呢?
效率能有多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
德州仪器 (TI) 宣布推出业内最小的离线相位可调光式恒流照明控制器和一款易用型照明驱动器,简化了多种LED灯泡(包括E14、GU10、A19、PAR20/30/38、MR16和AR111)的改型过程。TPS92075控制器和TPS92560驱动器可在减少元件数量、缩小解决方案尺寸的同时,提高与传统照明控制装置的兼容性。如欲了解更多信息或获取样品,敬请访问 www.ti.com.cn/tps92560-pr-cn 及 www.ti.com.cn/tps92075-pr-cn 。
首先DEMO是DEMO的问题,我们客户这边肯定有一些数据和DEMO是不一样的,比如我们需要做到16W,而DEMO做到10W,采用SEPIC.问题来了
1、TPS92560是否AC输入电压范围是否可以从9-15VAC
2、TPS92560是否可以在电子变压器前端加TRIAC,来调光
3、TPS92560的开关频率的选择,我有看到规格书建议使用电子变压器时我们频率点设在1MHZ-1.5MHZ,假如我使用电感式变压器我不需要这么大的频率,那么这颗IC的最低频率为多少?我们都知道频率越高我FCC过的难度就越大。