This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145 DCDC 输入24V 输出电压5V 输出电流最大只能到11A

Other Parts Discussed in Thread: LM5145, LM5145EVM-HD-20A

采用LM5145 设计的一个24V输入5V/15A 输出的电源,原理图以及PCB严格参考 LM5145EVM-HD-20A 评估板设计的以下是原理图和PCB,负载接入大功率可变陶瓷功率电阻,逐渐减小负载阻值输出电路增加输出电压稳定在4.98V,当输出电流超过11A时输出电压急剧下降至2V左右并发出呲呲生,增大负载阻值使电流小于11A时,电压又恢复正常,请问这个主要是什么原因造成的。

  • Hi
    首先你要确认电流保护,按照datasheet 第23/24页,注意要考虑MOS温度对于Rdson的影响,可以将电流保护点略微放宽一点。
    其次,不建议用陶瓷电阻负载,而建议用电子负载,前者可能存在一定寄生参数影响测试准确性。
    还有,你需要确认功率电感饱和电流足够,建议用20A以上饱和电流的功率电感。
    这些都确认没有问题的,再确认layout。
x 出现错误。请重试或与管理员联系。