This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606测试过程中相关问题



1,我设置2A最大充电电流充电,电池是3300mah的,开始充电时电池电压3.2V,充电时已2A充电不到1分钟电流还是下降,20min后下降到1A,此时断电后电池电压为3.8V。再上电后检测VSYS电压为4.173,说明电池很早就进入了恒压充电,实际恒流充电时间很短,导致充电时间长达4小时。我想询问的是这个恒流时间是电池决定还是芯片决定的,能延长这个恒流充电时间吗?

2,在系统空载情况下(关机),充电能在设置的2×5%=100mA处完成,STAT会自动拉高。电池带负载工作的情况下,插入适配器,负载供电能从电池切换为适配器供电,但是电池充电电流到达50mA也没有停止充电,stat一直为低电平,这是为什么?

3,这款芯片要做到OTG自动适应,是不是需要外部使能OTG管脚。

麻烦TI工程师帮忙解答这些天的疑惑。