Other Parts Discussed in Thread: LM76003
项目中用到TI的LM76003电源芯片,通过与数字电位器相连实现固定几个档位的电压输出,目前发现存在电源芯片击穿烧毁的情况,而且都出现了输出端(即SW与GND之间的短路现象)。采用的数字电位器默认上电是5K欧姆,具体原理图如下图所示。麻烦各位帮忙看一下,电路设计是否存在不合理的地方,谢谢!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM76003
项目中用到TI的LM76003电源芯片,通过与数字电位器相连实现固定几个档位的电压输出,目前发现存在电源芯片击穿烧毁的情况,而且都出现了输出端(即SW与GND之间的短路现象)。采用的数字电位器默认上电是5K欧姆,具体原理图如下图所示。麻烦各位帮忙看一下,电路设计是否存在不合理的地方,谢谢!!
谢谢您的回复。这里调压精度要求不高,主要是想不明白为什么会出现电源芯片炸了的现象。
你好,
这里做调压是为了设置直流风扇不同的转速工作,目前是设置成了三个档位,所以精度要求不高。
你好,
1、 请问电感是选用饱和电流8A以上,还是Irms 8A以上的?
2、如果只加大输出电容的容值C64,应该会加快负载响应,通过电感的电流是不是就变小了?就目前的情况,这个电容选多大合适?
3、因为实际用电流钳抓到的瞬态电流最大就4A,风扇最大转速时的工作电流是0.35A。但如果确实是电感饱和导致的失效,那这个电流肯定在6A以上,那LM76003能否满足当前场景的应用?您说的最高保护点是6.8A,是不是下图中的上管短路电流?目前失效的都是SW与GND短路,应该是下管短路了,电流超过5.3A多长时间会导致这种击穿失效?电源芯片自身的保护是指在这个最高保护点以下都还可以正常工作还是有一定时间要求?谢谢!
您好,
1、您说的一般1000uF以上,是指的我原理图中C64的输出电容吗?如果加大这个容值起不到优化的作用的话,那就维持现在22uf的容值,可以吗?
2、LM76003推荐最大输出电流3.5A,是否需要更换支持更大输出电流的BUCK?
3、由于一直怀疑是瞬态过流导致的失效,所以一直用电流钳进行电流的监测风扇的工作电流。之前调压是直接从30V到38V,或者从30V直接到45V,瞬态电流确实比较大,最恶劣的情况下在3.5A~4A左右。后续优化了 方案,需要从30V升至38V的时候,改成每隔500ms升到1V的策略,从瞬态电流来看确实优化了很多,最恶劣情况下在2A左右。感觉离电感饱和电流还差的很多,不知道为什么电源芯片还会失效?有可能是反向电流的问题吗?下表中最大3.3A吗?
下午用示波器监测了一下调压过程,并没特别明显的震荡变化。是按照预计的1v1v的升降。最大的瞬态电流也还是在调压过程中出现的。最大在2A。还是不明白为什么会让电感进入饱和