TLV62095输入3.3V,输出1V带不起负载,设置输出电压1.2V就可以带4A负载都没有问题,设置输出电压1.1V可以带到2.1A,然后电压掉到1V,再调高负载输出就跟不上了,我看手册最低输出是0.8V,我是按手册推荐电路做的,1uH电感,26mΩ5.8A,下周我试下TPS62095看能不能带负载正常输出1V。各位前辈有遇到过我这种情况的么,怎么解决呢?我需要输入3.3V输出1V4A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
能够输出1.2V/4A,说明你的功率电感饱和电流至少超过4.6A, 而下调0.1V, 负载能力大幅度下降,建议你确认一下你的layout。
参考datasheet第17页, 一般主要影响带载能力的原因是功率电感饱和电流不足,其次就是layout, 注意功率回路尽量小等等。
有按照手册推荐的来布局,它这个带不动负载的情况是输出1V的时候连10ma都带不了,输出1.05V,1.1V的时候随着负载增大输出电压下降,降到1.003V之后电流就上不去了。输出1.2V的时候可以带到4A,电压都还有1.1几伏,再高就没有测了。输出低于1V的情况我倒还没有试,我怀疑都不能输出低于1V的电压
找到问题的原因了,是我那台电子负载有问题,低于1V电压不能正常测量,换了另外一台设备现在测量正常了,输出到5.5A会保护。