最近项目使用TPS2420做过流保护,发现过流不符合预期,使用官方DEMO板测试也不符合预期,具体如下图(使用官方DEMO板测试),黄色一通道是电流(通过0.1Ω电阻串联测分压,即100mV对应1A电流),蓝色二通道是CT脚,对DEMO板用12V上电后正常输出12V,官方DEMO设置的保护电流是4A,故我们将负载仪设置为4.1A然后打开负载,可以看到在CT设置的时间内(DEMO板设置约22.5ms),板卡正常流过4.1A电流,然后保护关断,CT脚电容循环充放电尝试恢复正常导通,由于负载仪始终打开为4.1A负载,故每次都启动失败,按照手册描述,每次尝试启动的Tfault时间内,板卡应该按照4.1A电流导通,但是实测除了第一次是按照手册预期的4.1A外,其他时候都是只有0.5A左右电流导通;另外如果先将负载仪的4.1A负载打开,然后再给DEMO板上电,实测每次尝试启动的Tfault时间内,导通电流也是0.5A左右,还请帮忙分析原因,谢谢
此次申请的DEMO板还有TPS2421-1的,实测也是和TPS2420一样,先开负载再上电,Tfault时间内导通电流为0.5A左右;先上电正常工作后,再打开负载,过流是4.1A,但是TPS2421-1没有自动恢复功能,使用板卡上面的EN拨动开关手动尝试恢复,每次导通电流也只有0.5A左右