Other Parts Discussed in Thread: TPS563231, NE5532, LM2776, TPS62130, TPS63710, TPS54160, TPS5430
我们用12伏电源做主电源,通过TPS563231转成正5伏,再通过LM2776转成负5伏,给NE5532供电,问题是NE5532最低电压是正负5负,请问这种设计有没问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
如果负载不重(例如几十mA),对输出电压精度要求不高是可以的。 因为5V输入,转出来如果电流较大,例如100mA以上,输出电压会低于-4.8V,甚至更低。
你可以用降压芯片来做。例如TPS62130系列或者其他,直接用降压芯片+耦合电感来做,用12V输出正负5V. 依据电流需求选择TPS621xx版本。
谢谢您,我想问有没有芯片,可以把+12伏转成-12伏,这样就不用考虑负载的问题,我们设备电源12伏2安,有一块3.3伏TM32处理芯片,NE5532用在音频信号放大上面。多谢了