This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基准电压芯片LM4040分压问题

Other Parts Discussed in Thread: LM4040

期望得到1V左右的基准电压,所以对LM4040输出的2.048v电压进行分压,电路图如下所示

但对U2点电压进行测量,发现电压值几乎为0.08V左右,对LM4040的1脚进行测量,电压值也在零点零几V。请问这是为什么?如果想得到1V的基准电压,该如何改动?

  • Hi
    按照你5V输入,4V输出,50ohm上电流18V, 2mA流向2个1k电阻, 18mA太大, 建议你将50mhm电阻至少放大到100ohm以上(小于200ohm)
    然后再单独测试Vcc这里电压,如果还是很低,可能是芯片坏掉了。
  • Hi
    按照你5V输入,4V输出,50ohm上电流18V, 2mA流向2个1k电阻, 18mA太大, 建议你将50mhm电阻至少放大到100ohm以上(小于200ohm)
    然后再单独测试Vcc这里电压,如果还是很低,可能是芯片坏掉了。