你好!我们客户有一款产品用到了电池管理芯片BQ4050,在开发过程中发现了一些问题,需要您的协助!十分感谢!
1、我们的电池是四串两并的,电池充满的时候应该是接近16.8V左右,不知道为什么,有时候放电的时候,容量百分比有骤降的情况(比如:突然从90%以上突然降到10%以下,甚至是0%。重新烧录firmware容量又恢复到90%以上,但是不能彻底解决这个问题)
2、充电电流不准,我们用Battery Management Studio观察充电时的电压和电流,外部电源提供的充电电压是24V,电流是1A左右,而观察到Battery Management Studio上显示的电压是14V左右,电流却是2A多,明显大于真实的电流。
3、有时候在充电,容量百分比到了一定大小就充不进去了,但是显示的容量百分比还没达到100%,可能只有70%多。
4、我用模拟SMBus跟BQ4050通讯,正常情况下都可以正常通讯,但是偶尔会通讯不上,或者当我发一个指令获取一个参数(比如电流,电压等)获取到的是0xFF,0xFF,请问是否有什么方法可以优化代码?