Other Parts Discussed in Thread: UCC3895, UCC28950
TI的技术专家好
目前我在使用UCC3895设计ZVS超声波电源,针对官方资料中的参考设计有些疑问,希望解答一下
1、在峰值电流模式下,CS引脚信号应该和主回路脉动电流一致吧,不能加大电容滤波成平直的直流电平信号吧?
2、datasheet参考设计(图24)电流中采样电阻RCS后加了一个低通滤波RLF(1KΩ)、CLF(330PF),之后并联电阻20.0(R31),这显然画错了吧,还是单位标错了,接这么小电阻不就相当于接地了
3、关于自适应死区的计算,datasheet中 8.2.2.10.5 Setting the Switching Delays 配图错了吧,不是UCC3895呀
4、我的设计中使用AD9833输出脉冲给SYNC引脚,用于控制频率,这里SYNC信号应该是个窄脉冲,这个脉冲宽度有要求吗,还是越窄越好
5、我想主电路工作频率20KHZ,也就是CT振荡频率40KHZ,官方资料上显示不支持这么低的频率,可是国内大量文献都写它可以工作在20KHZ左右,我想得到官方观点,该芯片是否可以工作在15~20khz频率范围?