This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ33606 的几个问题



  1. 想工作在FPWM模式,SYNC/MODE引脚需要接偏置电压,那么偏置电压需要多大可以使其工作在FPWM,范围是多少 

2.  9脚VCC在引脚介绍时写了不要接任何原件,但是在demo板子的原理图中接了一个电容到地,这个实际需要吗

3.  PGOOD_PU和PGOOD, 若不使用是否可以悬空,还是将一个电压接到PGOOD_PU上,PGOOD通过内部的100k上拉到高电平即可

4. 10脚 BIAS_SEL什么情况下需要使用,手册上没看的明白

  • Hi
    1. To select FPWM mode, connect the SYNC/MODE pin to a bias voltage or logic signal greater than 0.6 V. 从这段话看高于0.6V即可,但是建议高于2V.
    2. 接电容稳压是必须的。
    3. 可以悬空。PGOOD是外接100kohm电阻到PGOOD_PU, PGOOD_PU实际上是供电。
    4. 这个脚可以用来改善效率,当输入电压很高时,内部LDO功耗较大,通过这个脚外接输入电压可以减小芯片内部LDO功耗。