This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我在使用LM5005芯片将+24V转换成-16V电压时遇到了问题,烦请看到的工程师帮我解答。问题如下:
在焊接好LM5005及其周围的元器件后,初次上电时,用万用表测量,显示可以正常输出-16V的电压,再次上电时,用万用表测量电压变为-4.5V左右。检查了周围的元器件没有发现问题。下图是我的原理图和PCB,原理图参考的是WEBENCH Power Deisigner中的电路。
图1为我的原理图,设计参数是输入+24V,输出-16V,1A。
图1
图2为贵司WEBENCH Power Deisigner中的电路,我的原理图中元器件的参数与这个基本一致,肖特基二极管参数略有差别。
图2
图3为我的PCB上的LM5005部分
图3
图4为接了50R的负载时测量的-16V和GND间的波形,可以看到直流有效值仅为-5.13V
图4
图5为接了50R的负载时测量的LM5005的SW引脚处的波形,图6至图9均为该图放大后的波形。
图5
图6
图7
图8
图9