Other Parts Discussed in Thread: TPS54218, TPS62140A, TPS62150A
原理图如下:
目前有两个问题,
1.是软启动是否能设置成0.1ms,规格书推荐是的1-10ms;
2.comp管脚的参数要怎么定
3.按照下图的原理图输出,蓝色曲线为芯片输入端电流,电流会有震荡并有过冲。这个是否正常。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是作为LED driver,LED驱动电流是600mA和1A,后端电路被我删减了一部分,原理我是清楚的,目前电路也是通过IN197将采样电阻的电压放大,然后通过vsense反馈。现在主要就是comp补偿这块要如何计算。
或者说TI 是否有DCDC类型的恒流源并且响应速度比较快,,因为我的产品对功耗和速度要求比较高。
另外关于TPS54218软启动的问题可以先帮忙回答下。