焊接tps7a4700空载时固定输出5V正常,当负载增时,tps7a4700输出为-0.9V当增大输入点压后,输出正常,接着负载增加,输出有为负0.9V,当把负载全为空时,输入为5V,输出仅为3.5V,第一次焊接调试时,空载输入为5V时,输出为4.8V,不知为什么,是这个芯片坏掉了,用了好几个tps7a4700,有一个压降大于1V时,仍不能正常工作
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
焊接tps7a4700空载时固定输出5V正常,当负载增时,tps7a4700输出为-0.9V当增大输入点压后,输出正常,接着负载增加,输出有为负0.9V,当把负载全为空时,输入为5V,输出仅为3.5V,第一次焊接调试时,空载输入为5V时,输出为4.8V,不知为什么,是这个芯片坏掉了,用了好几个tps7a4700,有一个压降大于1V时,仍不能正常工作
Hi
正电压LDO输出负电压来了,先将你的电路贴上来看看? 其次你的芯片哪里买的?