This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25883的输入电流设置

Other Parts Discussed in Thread: BQ25883

您好,

我正在使用BQ25883芯片给7.4v双节锂电池充电。

使用可编程直流电源当做输入源(设置成5.2V@3A),如果不设置BQ25883内部寄存器的话,显示输入电流IBUS为485mA。

我的目的是提高充电速度,所以我就提高了输入电流,修改了寄存器IINDPM值,当把此值改得大一些时则会停止充电,电源端电流为0了,想问这是为什么?

如果方法不正确,如何操作。

寄存器I2C通信没有问题,可以正确读取和写入。