This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1中Design Energy参数的疑问



设计能量 = 设计容量 * 标称电压 / 设计能量缩放倍数;

设计容量 = 典型容量 * 并联电芯数;

1、这两条计算公式是否有问题?

2、这里的标称电压是指电芯的标称电压还是指电池组的标称电压(电芯的标称电压*串联电芯数)?

3、Design Energy参数是不是在Load Mode = 1、Load Select = 4时才用到?其他情况该参数没有任何作用?

  • 您好,计算公式没有问题,设计容量和设计能量都是单串cell,如果有并联再*并联数,不是pack电压。
    不是只有Load Mode = 1、Load Select = 4才用到,if the Load Mode is set to 1 and Load Select = 4, the Design Capacity cWh will be used by the firmware to update the FCC and RM.