This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一下:为什么BQ4050的过流保护超过设定值5A仍然不起作用

Other Parts Discussed in Thread: BQ4050

附过放电保护程序配置图及电路原理图

  • 发表后看不到图片,这里手动描述:OOC1配置的是-4000mA 2s、 OOC2配置的是-6000mA 1s、 OCC配置的是0mA 5S

    电路上没有用二级保护,PTC 和PTCEN是直接接了VSS ,FUSE通过10K电阻下拉到VSS
  • 您好,将设置改为默认是否能进入保护。
  • 感谢回复,我没有理解到您的意思,是不是将所有设置都改为默认。我查因的结果是采样电阻阻值太小导致的,我这里作出详细的说明与需要了解问题 : 测试时使用的是在一块成熟的电池包中得到的程序。按照手册给出的采样电阻范围,我选择了0.001Ω,负载测试仪设定的电流是1A,通过软件:Battery Management Studio读出电流只有223mA。明显BQ4050检测到的电流远远小于负载测试仪设定的1A电流。接着,保持负载测试仪设定的1A电流,令采样电阻的阻值接近0.004Ω后,通过软件:Battery Management Studio读出的电流为889mA,发现已经接近负载测试仪设定的1A电流了(我不太接受111mA的误差)。请问配置软件:Battery Management Studio是否可以设置采样电阻的阻值(因为我没有找到设置采样电阻阻值的地方,所以希望能从TI的工程师那里得到确定的答案),或者手册中给出的采样电阻阻值的范围0.001-0.003Ω是不是存在错误?
  • 您好,我看评估板的电路上用的就是0.001ohm的电阻,电流不准确,您校正一下是否能改善。
    数据手册推荐1-3mohm的电阻,建议使用推荐的检测电阻值。
  • 我现在是用0.012欧姆和0.008欧姆电阻并联后与电路连接,Battery Management Studio测到的电流(-986mA)与负载测试仪设定的电流(1A)非常接近,误差小于5%
  • 方便回答一下校准需要如何操作吗?

  • 您好,电流校正一般是用2A放电校正,电压校正是测量电池的电压。详细请参考评估板的用户手册。
    www.ti.com.cn/.../zhcu128.pdf