工作场合:
监控装置上照明使用,工作电压范围在36-75V直流,环境温度最恶劣可达40度.
带2排4个LED灯
采用TI芯片LM3402HV
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM3402/02HV开关稳压器特征如下:输入电压范围 6V~75V,采用降压稳压器的线路布局;可为发光二极管提供恒定的驱动电流,回授电压为200mV;当RON接脚处于低电位时,停机电流便会进一步降低;准确的PWM亮度控制;开关频率高达1MHz;设有磁滞功能,而且导通时间固定。因此,可以在整个输入电压范围内进行开关频率(FSW)控制
图中的LM3402/02HV开关稳压器设有专用的亮度控制(DIM)接脚,可以利用线性以及PWM输入信号准确控制亮度。利用发光二极管发光的照明系统普遍采用PWM的光暗控制方式控制灯光亮度,这个亮度控制方法已成为业界普遍采用的标准。只要调节正向发光二极管的电流,发光二极管的光线输出量便会按照线性方式增减,但大部分光线的波段会出现偏移现象。部分应用对颜色的要求并不十分严格,因此仍会采用线性的亮度控制方式,但汽车灯如煞车灯、液晶显示器背光以及直接显示的RGB发光二极管对亮度及色彩都有极严格的要求,因此这类应用一般都会采用PWM方式控制亮度。