This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355工作频率的变化问题

Other Parts Discussed in Thread: TPS53353
我们在测试TPS53353(输入12V,输出0.85V,RF通过124K欧姆电阻上拉至VREG)不同负载的工作频率时,发现以下问题:
1、该电源在板内实际使用时的实测最大电流也只有2.65A(瞬态),我们的原始设计电感值是0.54uH,此时测到的开关频率在669khz~762khz。这个频率范围并不满足手册中850Khz开关频率时对应的频率范围770khz~930khz。
2、当我们把电感从0.54uH改成1uH时,测到的开关频率在731khz~861khz。这个频率范围的最小值还没有达到770khz。
3、当我们把电感继续改大至2uH时,测到开关频率陡降至467khz~520khz。
补充说明:以上试验测试过程中,输出电压始终正常,开关频率也维持了一定程度上的稳定性。
我们就有以下这些疑问:
1、根据TPS53353手册中给出的频率范围,我们在实测开关频率时,是需要关注开关频率在诸多信号样本中测到的最小值和最大值吗?还是只需要关注开关频率从诸多测试样本中计算出的平均值?
2、为什么电感增大到2uH时,开关频率会陡降至500Khz?而不是延续之前的试验效果,可以继续提升开关频率?
3、手册中给出的开关频率范围究竟应该怎么理解?是否在那些频率之外的工作状态,就一定是有问题的?是否一定是需要优化和修改设计的?