This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100工作在EOS模式下,所有数据都正常,唯独没有电流数据。

Other Parts Discussed in Thread: BQ35100, BQSTUDIO, EV2400

To use STATE-OF-HEALTH mode, follow these steps:

1. Step 1: Set GE high to power up the BQ35100 gauge and wait for ALERT to go low due to INITCOMP = 1.

2. Step 2: Clear ALERT (read BatteryStatus()).

3. Step 3: Read any required data such as State-Of-Health() for the latest battery data.

4. Step 4: Optional: Send GAUGE_START().

5. Step 5: Optional: Send GAUGE_STOP(). At this point, Lifetime Data can be stored and any Threshold detection checks are run. This is only needed if these features are desired.

6. Step 6: Set GE low to power down the BQ35100 device.

按照这个步骤,其他数据都有,就是没有电流。怎么回事呢,我读取电流是按照读取电压那样,标准命令读取的。