您好,我使用的电池是Sanyo NCR18650GA(3450mAh),通过BQ34Z100-G1采集的数据,使用GPC工具获得的chemical ID推荐如下,下面也有Sanyo NCR18650GA的chemical ID 1580,但推荐的最佳ID是2348,对于BQ34Z100-G1来说我应该怎么选择哪个chemical ID?下面的警告是什么意思,是否可以忽略?
Chemistry ID selection tool, rev=2.5
Configuration used in present fit:
ProcessingType = 2
NumCellSeries = 7
ElapsedTimeColumn = 0
VoltageColumn = 1
CurrentColumn = 2
TemperatureColumn = 3
Best chemical ID : 2348 Best chemical ID max. deviation, % : 1.87
Summary of all IDs with max. DOD deviation below 3%
Chem ID max DOD error, % Max R deviation, ratio
2348 1.87 0.67
2006 1.9 0.3
2101 1.93 0.75
2152 1.94 0.62
2142 1.95 0.42
2437 1.98 0.55
2050 2.01 0.29
2039 2.18 0.25
508 2.18 0.82
5167 2.26 0.49
2591 2.53 0.61
2588 2.54 0.62
2380 2.62 0.63
2125 2.63 0.81
2158 2.69 0.65
2250 2.71 0.82
2133 2.72 0.33
1580 2.73 0.58
2112 2.74 0.84
2107 2.74 0.98
1762 2.77 2.54
3758 2.81 0.72
2124 2.93 0.73
2150 2.96 0.92
Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.
Selection of best generic ID for ROM based devices like bq274xx
Device / Family #1
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
3142 bq27421-G1D: 4.4V LiCoO2 17.55
354 bq27411-G1C: 4.35V LiCoO2 19.64
312 bq27421-G1B: 4.3V LiCoO2 31.4
128 bq27421-G1A: 4.2V LiCoO2 100.05
Best generic ID 3142
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule
Device / Family #2
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 18.7
354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 19.64
1202 bq27621: (default) 4.2V LiCoO2 19.88
Best generic ID 1210
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule
Device / Family #3
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 17.55
3230 bq27426: (default) 4.35V LiCoO2 19.43
1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 19.88
Best generic ID 3142
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule