This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用TPS26400RHFR,请教一下其中管脚的问题以及我的用法是否合理?



板子上一共使用了两片TPS26400,一个用于板子的电源接入部分,使用其防反接,UVLO,和OVP, ILimit,以及IMon特性,设定正常输入最大值为24V,过载保护阈值26V,欠压锁定电压6V,最大电流2A,其中应用图如下

其中IMON引脚接到单片机的ADC引脚,SHDN,FLT悬空

还有一种应用,对外可控制输出板子的输入电源,类似外接传感器至主板,主板可以控制其电源的通断,类似于MOS管的用法,只是多了电流保护,以及外接传感器反接的保护。

请帮帮我评估一下这两种用法,非常感谢。

还有两个疑问,关于两种Mode的区别,Electronic circuit breaker with auto-retry和Active current limiting with auto-retry,我的理解是前者在大于IL的时候会直接断开连接,并不断重试,而后者会主动调节电流至IL并不断重试,不知道是否正确?

还有个关于Imon的理解,数据手册P25,

For IOUT > 50 mA, V(IMON) = [I(OUT) × GAIN(IMON)] × R(IMON)

For IOUT < 50 mA (typical), use Equation 7. V(IMON) = (I(IMON_ OS)) × R(IMON)

这句怎么理解呢,我监测我系统的动态功耗,我如何得知应该用哪个公式呢,因为我系统的电流有可能大于50ma 也有可能小于50ma,是不断在变化的