This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LED照明行业正慢慢复苏



开春以来,LED照明行业也是暖意阵阵。随着欧盟白炽灯全面禁止,LED照明应用进入质的变化阶段;国内在政府工程的推动下,商业照明、连锁照明有望加速渗透。

  据大众证券报报道,业界对今年的LED照明市场很是乐观。有人认为,受惠于一系列产业扶持政策,中国LED照明产业潜在市场巨大。根据统计,2009年至2013年,市场规模的复合增长率达到43.58%,预计到2013年我国LED照明市场规模有望达到730亿元。发改委近期发布了《半导体照明节能产业规划》,明确了促进LED照明节能产业产值年均增长30%左右,2015年达到4500亿元。

  目前中国照明需求规模庞大,2012年白炽灯和节能灯的大陆市场需求分别达到11.76亿只和12.69亿只,2007-2012年的年复合增长率达到7.59%,直管萤光灯的市场需求为8.3亿只,环形萤光灯的市场需求为8亿只,卤钨灯的市场需求为7.55亿只。分析认为,这些传统照明光源和灯具都是LED照明灯具的目标替代市场,随着性价比的提升,LED照明灯具将逐步进入这些市场领域,为其带来巨大的市场发展空间。

  • 国内一些大型LED企业对LED照明在户外和商业领域的前景颇为看好,他们认为,补贴政策将加快LED照明在户外和商业领域的推广。目前LED照明成本处于下降趋势,在户外和商业领域开始逐渐具有性价比的优势,需求保持快速增长。业内人士分析,从这次补贴政策来看,终端照明企业将直接获益于补贴政策,封装和芯片企业也可间接获益。有了补贴后,产品的性价比将会进一步提高,并将进一步拉动消费需求。乐观估计,如果今后参照节能灯的补贴幅度持续对LED进行财政补贴,LED照明的终端售价还会下降30%-50%,这将会极大刺激终端用户的需求。此外,政府招标中要求企业通过CQC的质量测试和节能认证,这也将有助于提升用户对LED照明品质的认可程度。总之,LED照明市场加速开启,国内LED行业将在未来几年内都保持稳定增长。
  • 现在的LED产业应用很广泛。