This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV766-Q1输出电流确认

Other Parts Discussed in Thread: TLV766-Q1

Hi All,

我这边想确认下,TLV766-Q1在输入为12V,输出5V条件下,即Vin-Vout=7V,此时输出电流为多大?能否达到500mA?

谢谢!

  • HI

        3.5W的功耗(电流达到500mA)意味着热阻必须减低,例如Junction-to-board thermal resistance  24.4℃/W,  否则芯片温度超标,除了过温保护还会大幅度降低可靠性。

        同时功耗大,效率低。  建议你选择DC/DC, 很多芯片效率都达到92%以上。  如果受限与空间,可以选择模块电源。如果考虑价格和空间,建议设法选择更低一些的输入源。