This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL494芯片输出问题

Other Parts Discussed in Thread: TL494

这个是boost电路一部分,在VCC是13.8V的情况下,为了同相输出,输出接的是TL494两个输出三极管的发射极,请问在发射极以及后面的推挽电路两次PN结压降以后还能不能驱动这个VGS需要4.7V的MOS管。主要是没看明白手册中Control这里,两个三极管基极电压是根据VCC来的还是根据VREF来的

  • 这个是boost电路一部分,在VCC是13.8V的情况下,为了同相输出,输出接的是TL494两个输出三极管的发射极,请问在发射极以及后面的推挽电路两次PN结压降以后还能不能驱动这个VGS需要4.7V的MOS管。主要是没看明白手册中Control这里,两个三极管基极电压是根据VCC来的还是根据VREF来的

  • Hi
    没有太明白你的意思。
    贴图在下面“使用高级编辑器编辑文本”的空间插入,否则我这边看不到。