This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] 【分享】BQ40Z80 常见问题

Other Parts Discussed in Thread: BQ40Z80

1,BQ40Z80 硬件保护时间问题

AOLD ASCD  能按照设置的参数保护,但是马上恢复,恢复时间设置的5S,实际测试发现是20mS。

原因是AFE充放电过流短路保护中,每个对应的一个RSVD_1, 默认是打开的,如果在配置参数时关掉了。 保护就立马恢复,不能打嗝。TRM 上介绍是do not use.

2, BQ40Z80 MAX ERRO 从1%变成101%

 循环学习OK 并且导出量产文件。 静置几天后发现MAX error变成101%

原因是在导出量产文件时,修改了cycle count ,没有修改Qmax cycle count ,只要对不上就会变成101%

3,Bq40z80充电过程不连接EV2300,即无SMBUS通信,延时几秒充电MOS关闭。

在测试过程中,发现上位机通过EV2300连接bq40z80时,可以正常进行充放电,各种状态寄存器也正常。去掉EV2300,延时几秒后,充电停止,此时充电MOS管关闭,放电MOS管打开,但Vgs电压比正常值低2V。这是什么方向问题?

原因是看门狗问题,没有检测到通信时,XCHG=1,禁止充电。不使能HWD就可以正常充放电。