This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25011接特定负载啸叫



24V转12V0.5A的DCDC电路,接纯阻性负载的时候没什么异常,但是接摄像头模组的时候就会出现很强烈的啸叫,实测电流0.155A。1、后来通过水泥电阻把电流调到0.15~0.16A并没有异常;
2、换一块PCBA有同样的现象;
3、换一颗摄像头模组正常,实测电流0.08A左右;
4、不用以下电路,而是用12V适配器供电,则没有啸叫。
  

故障输出电压波形如下图:(正常应该是稳定的12V,现在是6.5V有效值的三角波)
  
C73并联一颗100uF或者330uF电容后,先上电后接摄像头,则正常;先接摄像头后上电,则啸叫;
R79并联470pF电容后没有影响,还是会啸叫;