This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441电量计学习中FC一直无法置一

Other Parts Discussed in Thread: BQSTUDIO

电池容量是5900mAh,截止电压是4350,充满停充电压会降到4.24V左右,现在用bqstudio学习时候,发现设置如下参数一直FC一直不能置1,帮忙看一下具体问题

充满后,流到27441的电流,看bqstudio上面显示的电流为0,充满后我需要拔掉充电器吗,,因为电流为0,我看FC一直未置1,我也一直没有拔掉充电器

Dsg Current Threshold = 5900*10/167 = 353

Chg Current Threshold = 5900*10/100= 590

Quit Current = 5900 *10/73 = 808

Design Capacity = 5900

Design Energy = 5900*3.8

Terminate Voltage = 3400mV

Taper Rate = 5900*10/115 = 513

Taper Voltage = 120mv  充满后截止,电压会降到4.23V左右,所以用4350-4230=120mv

V at Chg Term = 4350mV

目前就配置了如上参数

BQ27441GB

  • 您好,taper voltage 的参数设置请参考TRM 6.4.2.3.11 Taper Rate, Taper Voltage

    Taper Voltage

  • 您的意思是我的taper voltage配置的不正确是吗?我可以理解为充电电压大于配置的Taper Voltage,为充满的条件之一
    充电的时候有看到电池电压4320,电流降为0后,电压直接降为4240,请问我是配置成多少,是配置成小于4320还是小于4240
    请问一下,其他的参数目前看起来可有异常?
    我看文档有介绍说是充电截止的判断条件
    Three requirements must be met to qualify for Primary Charge Termination:
    • During two consecutive periods of 40 seconds:
    IRateAvg1 < Taper Rate and IRateAvg2 < Taper Rate
    • During the same periods: Accumulated change in capacity per 40-second period
    • Voltage() > Taper Voltage
  • 您好,taper voltage 是定义检测充饱的最小电压阀值。TRM 推荐G1B = 4200
    其他参数没有看到问题。
  • 您好,我这边完成了bq27441的学习,但是学习完成后导入 gg.csv,发现插入充电器2A充电的情况,电量跳变挺大的,正常开机是8%,插入充电器开机就变成50%,这是为什么?而且学习成功了,我发现去读Ra_table的时候,发现ra_table还是之前的值,Qmax cell 0改变了

    2021-03-21 07:24:03 973 , Wr , AA , 61 , 1 , 00 

    2021-03-21 07:24:24 752 , Wr , AA , 3E , 1 , 58 

    2021-03-21 07:24:37 263 , Wr , AA , 3F , 1 , 00 

    2021-03-21 07:25:05 052 , Rd , AA , 40 , 33 , 00 10 00 11 00 14 00 18 00 14 00 12 00 14 00 14 00 15 00 16 00 18 00 1F 00 31 00 62 01 77 00 00 F7 

  • 您好,学习成功,请确认UpdateStatus的Bit 0 (0x01)and bit 1 (0x02)是否置1,置1表示 Qmax 和 Ra table更新成功。