This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24210太阳能充电问题



1、芯片EN引脚和PG引脚相连,BAT接4.2V锂电池,通过Iset电阻设定充电电流在390mA左右,无负载,当用数字电源作为VBUS时,锂电池电压小于3.6V时充电电流可以到一百多毫安,却达不到设定电流值。将锂电池电压大于3.6V的锂电池接上后,充电电流始终在1mA左右,请问什么原因?

2、当VBUS接太阳能电池板时,VDPM设置为5V左右,在阳光较弱或自然光下太阳能电池板输出功率较小时,上示波器后观测到EN引脚高低跳变,此时电池通过BAT引脚向芯片内部灌电流20——30μA,请问如何避免这种现象?

3、如问题1中EN引脚和PG引脚相连时,PG引脚不加上拉电阻应该也可以吧?