This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792充電參數設置問題

Other Parts Discussed in Thread: BQSTUDIO

您好:

 我們使用貴司的BQ25792設計了電池充電管理線路,出現以下問題,想請教一下:

1.REG03寄存器想要修改充電電流限值,嘗試了幾次均未修改成功,讀出的值一直為0xC8(我們是一個電池芯)

  我們的寫入方式應該是沒有問題,REG2E ADC_EN可以寫入OK

  修改充電電流ICHG這個參數有其他需要注意的事項嗎?不可以直接修改嗎?還是說電路的限流電阻就確定啦?

ICHG這個參數是不是對應著電池快速充電的電流呢?

2.充電過程中讀取的Battery電壓及充電中斷後讀取的電壓相差0.2V左右,如果要確認電池電壓是不是要先把CHG_EN關掉?不充電的時候讀取的電壓是相對較為準確的?

謝謝~~~~

  • 您好
    1,建议用BQSTUDIO试一下能不能修改成功。
    2,电压读取建议在充电停止以后,这样读取的电压准确。
  • 您好:

      請教一下充電停止多長時間讀取電壓比較準確?我們設計電池充電時會顯示充電進度條,某一時間讀取電池電壓時軟體控制充電停止1S,2S還是多長時間可以準確讀取電壓,計算出目前充電完成百分之幾?

     還有一個問題是我們修改REG08 IPRECHGB5:0為000010(80mA),確認可以修改成功,但是經過30s左右REG08 IPRECHGB5:0又變成了000011(120mA)

    這個不知道是為什麼?

     另外請教一下修改寄存器充電參數前有其他前提條件嗎?除了EN_CHG是Enable

     BQ STUDIO安裝後顯示:No free adapters are available for use on this system,讀寫寄存器時顯示ERROR

  • 您好,充电停止以后等电压不再下降这时就可以读取电压,时间建议您实际测量一下。
    参数设置以后30S恢复默认值请确认您的Watchdog timer settings
    修改参数请参考数据手册8.4 Device Functional Modes
    出现上述error请参考下面链接的解决办法。
    e2e.ti.com/.../bq76952evm-bqstudio-no-free-adapters-are-available-for-use-on-this-system