This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前寄存器信息如下:
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ?...............
10: 00 00 ff 00 55 55 55 55 d2 d4 d8 d0 ff 00 00 XX ....UUUU????...X
20: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXX
30: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX 00 XXXXXXXXXXXXXXX.
40: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXX
50: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX 00 XXXXXXXXXXXXXXX.
60: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXX
70: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXX
80: 81 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ?...............
90: 00 00 ff 00 55 55 55 55 d2 d4 d8 d0 ff 00 00 XX ....UUUU????...X
a0: a1 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ?...............
b0: 00 00 ff 00 55 55 55 55 d2 d4 d8 d0 ff 00 00 XX ....UUUU????...X
c0: c1 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ?...............
d0: 00 00 ff 00 55 55 55 55 d2 d4 d8 d0 ff 00 00 XX ....UUUU????...X
e0: e1 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ?...............
f0: 00 00 ff 00 55 55 55 55 d2 d4 d8 d0 ff 00 00 XX ....UUUU????...X
已经配置了MODE1为0x01,LEDOUT0~4全部是0x55,就是全部点亮,但是目前就是不亮,不知道什么问题了