This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952的Alert引脚输出和温度采样问题

Other Parts Discussed in Thread: BQ76952

(1)需求:AFE的全部AD采样完成后,在Alert引脚上输出高电平信号。

        现象:按照规格书上的配置说明,进行了配置,不能预期的效果,当修改它的有效电平,Alert引脚的输出电平也没有变化。

        疑问:都要配置哪些寄存器,需要怎么配置,是否说相关资料进行说明??

(2)需求:用T1、T2和T3进行温度采样。

       现象:T1的温度采样及读取是正常的,因此,我把T1的配置寄存器的值读回,并把这个值写入T3的配置寄储器中,可是仍然不能实现T2的温度采集功能;

       疑问:要实现采样功能,需要怎么配置。