问题1、我电池满电是4.35V、8000mah的,当电池放电时,比如说现在电压是3.7V,而我的负载1.6A(0.2C)的话,电压会拉低0.5V左右,那么现在电量计测到的电压就是3.2V,而我保护板的保护电压是2.9V,也就是说当保护板保护后,我的实际电压还有3.4V,这样学习的话放电电流是不是太大了,造成我压差很大,可不可以适当的降低放电电流,比如说前期大电流,后期小电流,到最后最大可能的接近3.0V
问题2、Ra FLAG是什么时候更新的,我现在已经充满电然后静置了2小时以上,update status变成了0x05,可是Ra FLAG还是0xff55,这是否正常,如果不正常,问题可能现在在哪?