在使用BQ25570时接入负载后电压变低,我输入为2.3V的直流电,在Vstor处接了一个470uF的电容,充电完毕后电容4.6v,Vout输出为3.3v(对R10进行了修改),但是接入负载后,Vout输出电压从3.3v降到60mV,这是什么原因呢?应该怎么处理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用BQ25570时接入负载后电压变低,我输入为2.3V的直流电,在Vstor处接了一个470uF的电容,充电完毕后电容4.6v,Vout输出为3.3v(对R10进行了修改),但是接入负载后,Vout输出电压从3.3v降到60mV,这是什么原因呢?应该怎么处理?
我是用振动生成的电压,整流后接到板子的输入端,在Vstor处外接一个1800uF的电容,最后输出接了一个5.6K的电阻,发现电容充电完毕也只有2.09V,然后输出端只有1.98V,并且电流很低。只有0.1mA。除此之外,我使用电流表测量电容两端电流后,电容的电压立刻归零,要重新充电。
PS:我将R10 进行过修改,致使Vout输出在空载时可达3.3V
输入功率是4.4mW,不过我这边重新弄了一下,发现是在负载测量时发生了短路问题,这个测量问题是解决了;
Vstor上我接的是一个2200uF的电容,负载是100K电阻